Download document () of 20
Eaton: UL 508A certification, UL 508A Zertifizierung

How does a control panel become UL 508A-compliant?

If machines and systems are to be exported to the US or Canada, the associated control panels must be constructed and certified in accordance with the regulations of UL 508A or CSA C22.2 No. 286. cUL certification for Canada also conforms to CSA (Canadian Standards Association) standards, which is why this certification is considered and recognized by the Canadian authorities as a CSA certification. UL and CSA are applicable in both markets. The technical details of the control panel are a crucial factor in attaining UL 508A compliance. Manufacturers should therefore already be taking the requirements of the standard into account during the project planning stages. In order to construct a control panel in accordance with UL 508A, each individual area should be adapted or designed according to the North American control panel standard.

Get our control panel design guide

1: Design of the feeder

Blogs_MOEM_UL508A_Graphic.jpg

The nominal current of the feeder is determined by the cumulative nominal currents of the branch circuits, such as the full load currents of motors and other loads.

When planning the feeder, it is also crucial that main switches (circuit breakers and molded case switches), which are equipped with door coupling rotary handles, have an additional rotary handle. Only then are the requirements of UL 508A fulfilled.

The rotary handels for main switches are an example for the differences between IEC and UL/CSA standards for control panel. It is important that main switches can only be operated by the intentional switching of an additional handle when the door is opened. To learn more read our white paper.
Moeller

2: Group protection for motor circuits

UL 508A includes provisions for protecting several motors with only one set of fuses or circuit breakers (section 31.4.1.c). However, all devices in the electrical circuit must be designed for group protection (this must be indicated on the devices or in the instructions).

In addition, the conductors for the individual loads must have a minimum nominal current of 1/10th the nominal current of the branch circuit protection used for the individual electrical circuits with manual motor controllers (MMC).

The MMC must be marked as "suitable as tap conductor protection in group installations." The conductors on the load side of the MMC must also have a minimum nominal current of 125 % of the full load amperes (FLA) of the motor.

When designing branch protection, the following values must be observed:

  • If the BCPD (branch circuit protective device) is a circuit breaker: 250 % of the largest motor's FLA plus the cumulative remaining motor loads.
  • If the BCPD is a time delay fuse: 175 % of the largest motor's FLA plus the cumulative remaining motor loads.
  • If the BCPD is a Class CC fuse: 300 % of the largest motor's FLA plus the cumulative remaining motor loads.

The nominal current of the BCP must not exceed the nominal current described in the component group protection marking and must correspond to the specified type.

icon_Linkedin_colored_256x256.png

Follow #EatonMachine on LinkedIn

Get every important blog post or new information Eaton is pulishing for machine and systembuilders. 

Blogs_MOEM_UL_CSA_Motorstarter.jpg

3: Single motor feeder

There are several ways to create a branch circuit for a motor feeder. Each of these methods includes short-circuit protection, overload protection and the ability to start and stop the motor. Some methods also include the ability to isolate the branch circuit for repair and maintenance purposes (disconnectors).

UL 508 Type F combination motor controllers (CMCs) are the most efficient solution for a branch circuit for a motor: They combine motor-protective circuit-breakers, contactors and feeder adaptors in one device.

4: Heating and lighting load circuits

The branch circuit protection for heating loads should:

  1. only use UL 489 circuit breakers or UL 248 time delay fuses (no combination motor controllers),
  2. not be less than 125 % of the heating load,
  3. not exceed 60 A and
  4. not exceed the nominal current of the wiring to the heating system.

The design of controllers (e.g. contactors) for heating control depends on the full load current of the heating system using the general purpose ratings or the resistive load ratings.

The branch circuit protection for normal incandescent lamp or fluorescent lamp loads should:

  1. only use UL 489 circuit breakers or UL 248 time delay fuses (no combination motor controllers),
  2. not exceed 20 A and
  3. not exceed the current of the intended wiring.
The design of controllers (e.g. contactors) corresponds to the respective nominal lighting values.
eaton-molded-case-circuit-breaker-PKZM4-image.jpg
The molded case circuit breaker PKZM4 is a real problem solver for the North American market.

5: Control circuits

Control circuits must be primarily protected in accordance with UL 508A. If the control circuit is built with a separate power supply, the following applies:

  • For single-phase power supplies, the need to use an additional
    fuse protection can be waived if the N-conductor is grounded.
  • However, the wire must be laid in a way that protects it from short circuits.
  • Otherwise, the L conductor requires a fuse protection.
  • Three-phase power supplies are protected by upstream fuse elements.
  • UL 508A requires time delay fuses or circuit breakers (verified according to UL 489) to be used where the control circuit branches off the feeder.

Fuse protection for "Class 1" and "Class 2" control circuits should be implemented according to Table 42.2 of UL 508A. Low-voltage limited energy circuits should be protected in accordance with the 100-VA rule using special time delay fuses or miniature circuit breakers.

6: Fuses

According to UL 508A, non-motor loads must be protected as specified by the respective manufacturer in the UL report. Circuit breakers compliant with UL 489 or fuses compliant with UL 248-4...12 must be used.

Fuses are additionally of interest because they can also be used to very easily increase the SCCR of the switchgear system so that it attains an SCCR that is compliant with the National Electric Code.

Blog_MOEM_UL508A_Fuses.jpg

7: Wiring

UL 508A also defines specific requirements for main and control current wiring, including the cross section, color and current carrying capacity.

Detailed information on this can be found in the "Design guide for control systems according to UL 508A," which can be downloaded from the Eaton website.

 

Conclusion

Machines that meet IEC standards are often exported to North America (the US and Canada). However, the codes and standards that must be adhered to in North America differ considerably from those in other regions of the world. For this reason, it is important for control panel manufacturers to take the requirements of UL 508A into consideration from the beginning, during the project planning stage. This will simplify commissioning and reduce costs later.

Control panel design guide according UL 508A

Our control panel design guide helps machine and system builder to design control cabinets for the North American market and to select the right products for their application.

Related posts