Machine production (most challenging phase)
The majority of machine builders (59%) surveyed* reported that the manufacturing stage is the most challenging part of the machine production cycle. This includes scheduling, assembling, fabricating and machine tooling.
Machine design (second most challenging phase)
More than half (56%) of respondents cited the design stage as the most challenging part of the process, followed by maintenance (39%), testing (33%), distribution and training (28% each), and end-of-life (22%).